ARKbase CE



Home



E-mail
has.software@onsemi.com




ARKbase CE v6.6.2
Readme File
Release Notes



ARK is a set of software building blocks that can help reduce the time it takes to develop hearing aid fitting software. ARKbase CE contains the core ARKbase DLLs compiled for operating systems based on Windows CE. A simple application, ParamsCE, is also included.


Important Installation Notes:

ARKbase CE is packaged as a self-extracting zip file. By default, it extracts to "c:\ARKCE".
To install the core ARKbase DLLs and ParamsCE, run SETUP.EXE from the ARKCE directory. This setup program will determine which device is connected and install the appropriate CAB file.

For more Installation Notes, please see the ARKbase CE Readme File.




Note:
Downloading any ARkbase CE software package from ON Semiconductor requires a login name, password and the proper download privileges. A login name and password can be created by registering with ARKonline™ here.




* ARKonline™ is a trademark of Semiconductor Components Industries, LLC.






Copyright © 2019 Semiconductor Components Industries, LLC